Testing and Debugging Automotive and Electronic Signals Using an Oscilloscope
 
January 21, 2020
 
Indiana Wesleyan University
4100 Rockside Road
Independence, OH 44131
 

This workshop will provide an extensive hands-on experience to test and debug automotive designs and other electronic signals using some of the advanced features and measurement capabilities of Keysight’s InfiniiVision 4000 X-Series Oscilloscope. Class sizes are limited to allow for 2-3 individuals per test station, so every participant will be able to experience the value of these oscilloscopes.

This workshop will cover the following:

  • InfiniiVision 4000 X-Series oscilloscope overview
  • Making measurements and using handy triggers
  • Decoding I2C & SPI signals
  • Decoding and triggering on the CAN bus at a hexadecimal level and using a .dbc file to symbolically decode and trigger on the CAN bus at a message and signal level
  • Using segmented memory acquisition to capture multiple and consecutive errors
  • Dual-bus “gateway” analysis (CAN and LIN)
 
Agenda:

8:30 a.m. - Registration and Refreshments
9:00 a.m. - Introduction and Hands-On Labs
11:00 a.m. - Conclusion

Co-sponsored by: