Testing and Debugging Automotive and Electronic Signals Using an Oscilloscope
 
January 22, 2020
 
Towne Place Suites by Marriott
2785 Freeport Rd
Pittsburgh, PA 15238
 

This workshop will provide an extensive hands-on experience to test and debug automotive designs and other electronic signals using some of the advanced features and measurement capabilities of Keysight’s InfiniiVision 4000 X-Series Oscilloscope. Class sizes are limited to allow for 2-3 individuals per test station, so every participant will be able to experience the value of these oscilloscopes.

This workshop will cover the following:

  • InfiniiVision 4000 X-Series oscilloscope overview
  • Making measurements and using handy triggers
  • Decoding I2C & SPI signals
  • Decoding and triggering on the CAN bus at a hexadecimal level and using a .dbc file to symbolically decode and trigger on the CAN bus at a message and signal level
  • Using segmented memory acquisition to capture multiple and consecutive errors
  • Dual-bus “gateway” analysis (CAN and LIN)
 
Agenda:

8:30 a.m. - Registration and Refreshments
9:00 a.m. - Introduction and Hands-On Labs
11:00 a.m. - Conclusion

Co-sponsored by: